AxesMap Struct
An array used for properly mapping Virtual Group axes to the Real Group axes. Currently Compass is set up for controlling 5 axes (X, Y, Z, Aux1, Tangent), Virtual Group is set up accordingly and should not be modified. The actual axes on the machine might differ so using this array you can disable non existing axes and properly point virtual axes to the real axes.
| Name | Data Type | Description |
|---|---|---|
| AxesMap[1] | INT | Virtual X axis |
| AxesMap[2] | INT | Virtual Y axis |
| AxesMap[3] | INT | Virtual Z axis |
| AxesMap[4] | INT | Virtual Aux1 axis |
| AxesMap[5] | INT | Virtual Tangent axis |
Router real axis group is set up for 4 axes (5 including X prime):
RealC axis is used as a Tangent axis, so the AxisMap is set up like this: