-

Prerequisites

Required Hardware Components

    • Yaskawa iC9200 series iCube MC motion controller licensed for at least 8 axes
    • Yaskawa SERVOPACKs and motors as required
    • Yaskawa SLIO IO modules as required
    • Industrial PC
    • USB license dongle for Compass Designer

Required Software Components

    • iCube Engineer
    • Compass 2 iCube Engineer Starter Project
      • NOTE: While extracting the starter project, select "Override existing file" for the "CompassComms" and "Y_Compass_Toolbox" in the Open Archive dialog.
    • Compass Designer
      • NOTE: The Compass Designer's starter project, used in this Getting Started section, is included in the Compass Designer's download. No separate files are needed.

Performance-related Requirements

Software

Network

Industrial PC Specifications



Requirements vary depending on individual application requirements, but the recommendations below work well for most applications:

PC specifications for enhanced performance:



 


This is the latest version of Compass Online help and the content may refer to features not available in previously released versions of Compass.

Copyright © 2026 YASKAWA America, Inc.